Package | Description |
---|---|
nxopen.facet |
Provides classes and interfaces for Faceted Representations.
|
Modifier and Type | Field and Description |
---|---|
static BridgeFacetBodyBuilder.Input |
BridgeFacetBodyBuilder.Input.DELETE
Delete the input facet body after builder committing
|
static BridgeFacetBodyBuilder.Input |
BridgeFacetBodyBuilder.Input.HIDE
Hide the input facet body after builder committing
|
static BridgeFacetBodyBuilder.Input |
BridgeFacetBodyBuilder.Input.KEEP
Keep the input facet body after builder committing
|
Modifier and Type | Method and Description |
---|---|
BridgeFacetBodyBuilder.Input |
BridgeFacetBodyBuilder.inputStatus()
Returns the option to specify how to deal with the input two facet bodies: keep, delete or hide
License requirements: None. |
static BridgeFacetBodyBuilder.Input |
BridgeFacetBodyBuilder.Input.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeFacetBodyBuilder.Input |
BridgeFacetBodyBuilder.Input.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeFacetBodyBuilder.Input[] |
BridgeFacetBodyBuilder.Input.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeFacetBodyBuilder.setInputStatus(BridgeFacetBodyBuilder.Input inputStatus)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.