Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse.ALWAYS_CREATE_NEW_DATA
This option will always create new data
|
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse.ALWAYS_USE_EXISTING_DATA
This option will use existing data to overlay
|
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse.ASKAT_RUNTIME
This option tells to show messages at rumtime
|
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse.CREATE_NEW_DATAIF_NONE_EXISTS
This option will create new data if none exists
|
Modifier and Type | Method and Description |
---|---|
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse |
VisualDrawingComparePrefsBuilder.overlayDataToUse()
Returns the overlay data to use
License requirements: None. |
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse[] |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
VisualDrawingComparePrefsBuilder.setOverlayDataToUse(VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsOverlayDataToUse overlayDataToUse)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.