Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType.AGAINST_ANOTHER_DRAWING
This option is used to overlay different part over current part
|
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType.AGAINST_OVERLAY_DATAIN_ACTIVE_DRAWING
This option is used to overlay current part on itself
|
Modifier and Type | Method and Description |
---|---|
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType |
VisualDrawingComparePrefsBuilder.compareMethodType()
Returns the compare method type
License requirements: None. |
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType[] |
VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
VisualDrawingComparePrefsBuilder.setCompareMethodType(VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType compareMethodType)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.