Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static ViewWorkflowBuilder.Display |
ViewWorkflowBuilder.Display.CURVES_ONLY |
static ViewWorkflowBuilder.Display |
ViewWorkflowBuilder.Display.DISPLAYAND_EMPHASIZE |
Modifier and Type | Method and Description |
---|---|
ViewWorkflowBuilder.Display |
ViewWorkflowBuilder.faceDisplay()
Returns the face display provides options in an extracted edge view that are available for selection
License requirements: None. |
static ViewWorkflowBuilder.Display |
ViewWorkflowBuilder.Display.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewWorkflowBuilder.Display |
ViewWorkflowBuilder.Display.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewWorkflowBuilder.Display[] |
ViewWorkflowBuilder.Display.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ViewWorkflowBuilder.setFaceDisplay(ViewWorkflowBuilder.Display faceDisplay)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.