Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Method and Description |
---|---|
ViewStyleShipbuildingLinesBuilder |
DraftingViewCollection.createShipbuildingLineBuilder()
Creates a
ViewStyleShipbuildingLinesBuilder
License requirements: drafting ("DRAFTING") Created in NX8.0.0 |
ViewStyleShipbuildingLinesBuilder |
ViewStyleShipbuildingLinesBuilderList.findItem(int index)
Returns the object at the input index.
|
ViewStyleShipbuildingLinesBuilder[] |
ViewStyleShipbuildingLinesBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ViewStyleShipbuildingLinesBuilderList.append(ViewStyleShipbuildingLinesBuilder object)
Appends an object to the list
License requirements: None. |
void |
ViewStyleShipbuildingLinesBuilderList.append(ViewStyleShipbuildingLinesBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ViewStyleShipbuildingLinesBuilderList.erase(ViewStyleShipbuildingLinesBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ViewStyleShipbuildingLinesBuilderList.erase(ViewStyleShipbuildingLinesBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ViewStyleShipbuildingLinesBuilderList.findIndex(ViewStyleShipbuildingLinesBuilder obj)
Finds the index where the input object appears.
|
void |
ViewStyleShipbuildingLinesBuilderList.insert(int location,
ViewStyleShipbuildingLinesBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ViewStyleShipbuildingLinesBuilderList.setContents(ViewStyleShipbuildingLinesBuilder[] objects)
Sets the contents of the entire list.
|
void |
ViewStyleShipbuildingLinesBuilderList.swap(ViewStyleShipbuildingLinesBuilder object1,
ViewStyleShipbuildingLinesBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.