Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static ViewSectionLineBuilder.ShowSectionLineType |
ViewSectionLineBuilder.ShowSectionLineType.WITH_SECTION_VIEW |
static ViewSectionLineBuilder.ShowSectionLineType |
ViewSectionLineBuilder.ShowSectionLineType.WITHOUT_SECTION_VIEW |
Modifier and Type | Method and Description |
---|---|
ViewSectionLineBuilder.ShowSectionLineType |
ViewSectionLineBuilder.showSectionLine()
Returns the value to show section line with or without view
License requirements: None. |
static ViewSectionLineBuilder.ShowSectionLineType |
ViewSectionLineBuilder.ShowSectionLineType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewSectionLineBuilder.ShowSectionLineType |
ViewSectionLineBuilder.ShowSectionLineType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewSectionLineBuilder.ShowSectionLineType[] |
ViewSectionLineBuilder.ShowSectionLineType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ViewSectionLineBuilder.setShowSectionLine(ViewSectionLineBuilder.ShowSectionLineType showSectionLine)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.