Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static ViewProjectionBuilder.Types |
ViewProjectionBuilder.Types.PROJECT_ON_ONE_PLANE
on one plane
|
static ViewProjectionBuilder.Types |
ViewProjectionBuilder.Types.PROJECT_ON_TWO_PLANES
on two planes
|
Modifier and Type | Method and Description |
---|---|
ViewProjectionBuilder.Types |
ViewProjectionBuilder.type()
Returns the type of the view projection
License requirements: None. |
static ViewProjectionBuilder.Types |
ViewProjectionBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewProjectionBuilder.Types |
ViewProjectionBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewProjectionBuilder.Types[] |
ViewProjectionBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ViewProjectionBuilder.setType(ViewProjectionBuilder.Types type)
License requirements: nx_layout ("NX Layout") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.