Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static ViewDetailLabelBuilder.LabelParentTextPlacement |
ViewDetailLabelBuilder.LabelParentTextPlacement.ABOVE_STUB |
static ViewDetailLabelBuilder.LabelParentTextPlacement |
ViewDetailLabelBuilder.LabelParentTextPlacement.BEFORE_OR_AFTER_STUB |
Modifier and Type | Method and Description |
---|---|
ViewDetailLabelBuilder.LabelParentTextPlacement |
ViewDetailLabelBuilder.textPlacement()
Returns the text placement
License requirements: None. |
static ViewDetailLabelBuilder.LabelParentTextPlacement |
ViewDetailLabelBuilder.LabelParentTextPlacement.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewDetailLabelBuilder.LabelParentTextPlacement |
ViewDetailLabelBuilder.LabelParentTextPlacement.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewDetailLabelBuilder.LabelParentTextPlacement[] |
ViewDetailLabelBuilder.LabelParentTextPlacement.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ViewDetailLabelBuilder.setTextPlacement(ViewDetailLabelBuilder.LabelParentTextPlacement textPlacement)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.