Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static ViewCommonViewLabelBuilder.SecondaryAlignmentType |
ViewCommonViewLabelBuilder.SecondaryAlignmentType.INLINE |
static ViewCommonViewLabelBuilder.SecondaryAlignmentType |
ViewCommonViewLabelBuilder.SecondaryAlignmentType.SUBSCRIPT |
Modifier and Type | Method and Description |
---|---|
ViewCommonViewLabelBuilder.SecondaryAlignmentType |
ViewCommonViewLabelBuilder.secondaryAlignment()
Returns the secondary alignment
License requirements: None. |
static ViewCommonViewLabelBuilder.SecondaryAlignmentType |
ViewCommonViewLabelBuilder.SecondaryAlignmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewCommonViewLabelBuilder.SecondaryAlignmentType |
ViewCommonViewLabelBuilder.SecondaryAlignmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewCommonViewLabelBuilder.SecondaryAlignmentType[] |
ViewCommonViewLabelBuilder.SecondaryAlignmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ViewCommonViewLabelBuilder.setSecondaryAlignment(ViewCommonViewLabelBuilder.SecondaryAlignmentType secondaryAlignment)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.