Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static TrackDrawingChangesGeneralBuilder.CompareMethodType |
TrackDrawingChangesGeneralBuilder.CompareMethodType.AGAINST_ANOTHER_DRAWING
This option is used to compare different part over current part
|
static TrackDrawingChangesGeneralBuilder.CompareMethodType |
TrackDrawingChangesGeneralBuilder.CompareMethodType.AGAINST_SNAPSHOT_DATA_IN_ACTIVE_DRAWING
This option is used to compare current part on itself
|
static TrackDrawingChangesGeneralBuilder.CompareMethodType |
TrackDrawingChangesGeneralBuilder.CompareMethodType.OPEN_SAVED_COMPARISON_REPORT
This option is used to open a compare report that is saved in the current part
|
Modifier and Type | Method and Description |
---|---|
TrackDrawingChangesGeneralBuilder.CompareMethodType |
TrackDrawingChangesGeneralBuilder.compareMethod()
Returns the compare method
License requirements: None. |
static TrackDrawingChangesGeneralBuilder.CompareMethodType |
TrackDrawingChangesGeneralBuilder.CompareMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrackDrawingChangesGeneralBuilder.CompareMethodType |
TrackDrawingChangesGeneralBuilder.CompareMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrackDrawingChangesGeneralBuilder.CompareMethodType[] |
TrackDrawingChangesGeneralBuilder.CompareMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrackDrawingChangesGeneralBuilder.setCompareMethod(TrackDrawingChangesGeneralBuilder.CompareMethodType compareMethod)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.