Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType |
TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType.SNAPSHOT |
static TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType |
TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType.TRACKED_CHANGES |
Modifier and Type | Method and Description |
---|---|
TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType |
TrackDrawingChangesGeneralBuilder.baselineOfComparison()
Returns the baseline of comparison
License requirements: None. |
static TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType |
TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType |
TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType[] |
TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrackDrawingChangesGeneralBuilder.setBaselineOfComparison(TrackDrawingChangesGeneralBuilder.BaselineOfComparisonType baselineOfComparison)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.