Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static StandardViewsBuilder.Placement |
StandardViewsBuilder.Placement.CENTER |
static StandardViewsBuilder.Placement |
StandardViewsBuilder.Placement.CORNER |
Modifier and Type | Method and Description |
---|---|
StandardViewsBuilder.Placement |
StandardViewsBuilder.placementType()
Deprecated.
Deprecated in NX6.0.2. Use the type of the multiple view placement
|
static StandardViewsBuilder.Placement |
StandardViewsBuilder.Placement.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StandardViewsBuilder.Placement |
StandardViewsBuilder.Placement.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StandardViewsBuilder.Placement[] |
StandardViewsBuilder.Placement.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StandardViewsBuilder.setPlacementType(StandardViewsBuilder.Placement type)
Deprecated.
Deprecated in NX6.0.2. Use the type of the multiple view placement
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.