Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static SketchSectionLineBuilder.SectionLineTypes |
SketchSectionLineBuilder.SectionLineTypes.HALF |
static SketchSectionLineBuilder.SectionLineTypes |
SketchSectionLineBuilder.SectionLineTypes.POIN_TO_POINT |
static SketchSectionLineBuilder.SectionLineTypes |
SketchSectionLineBuilder.SectionLineTypes.SIMPLE_STEPPED |
Modifier and Type | Method and Description |
---|---|
SketchSectionLineBuilder.SectionLineTypes |
SketchSectionLineBuilder.sectionLineType()
Returns the section line type
License requirements: None. |
static SketchSectionLineBuilder.SectionLineTypes |
SketchSectionLineBuilder.SectionLineTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchSectionLineBuilder.SectionLineTypes |
SketchSectionLineBuilder.SectionLineTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchSectionLineBuilder.SectionLineTypes[] |
SketchSectionLineBuilder.SectionLineTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SketchSectionLineBuilder.setSectionLineType(SketchSectionLineBuilder.SectionLineTypes sectionLineType)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.