Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Method and Description |
---|---|
SectionLineSegmentPointBuilder |
SectionLineSegmentPointListBuilder.addCutSegment(Point location)
Creates a new
SectionLineSegmentPointBuilder object
License requirements: None. |
SectionLineSegmentPointBuilder |
SectionLineSegmentPointListBuilder.addCutSegment(Point location,
SectionLineSegmentPointBuilder referencedCutSegment)
Creates a new
SectionLineSegmentPointBuilder
In case of point to point section line ,new segment is added at location prior to reference cut segment specified. |
SectionLineSegmentPointBuilder |
SectionLineSegmentPointListBuilder.createSectionLineSegmentPointBuilder()
Creates a new
SectionLineSegmentPointBuilder object
License requirements: None. |
SectionLineSegmentPointBuilder |
SectionLineSegmentPointListBuilder.findItem(int index)
Returns
SectionLineSegmentPointBuilder object at the input index. |
SectionLineSegmentPointBuilder[] |
SectionLineSegmentPointListBuilder.getContents()
Queries all the
SectionLineSegmentPointBuilder objects
License requirements: drafting ("DRAFTING") Created in NX10.0.0 |
Modifier and Type | Method and Description |
---|---|
SectionLineSegmentPointBuilder |
SectionLineSegmentPointListBuilder.addCutSegment(Point location,
SectionLineSegmentPointBuilder referencedCutSegment)
Creates a new
SectionLineSegmentPointBuilder
In case of point to point section line ,new segment is added at location prior to reference cut segment specified. |
void |
SectionLineSegmentPointListBuilder.append(SectionLineSegmentPointBuilder pointData)
Appends
SectionLineSegmentPointBuilder object to the end of the list
License requirements: drafting ("DRAFTING") Created in NX10.0.0 |
void |
SectionLineSegmentPointListBuilder.delete(SectionLineSegmentPointBuilder point)
Deletes a given
SectionLineSegmentPointBuilder object from the list
License requirements: drafting ("DRAFTING") Created in NX10.0.0 |
int |
SectionLineSegmentPointListBuilder.getIndex(SectionLineSegmentPointBuilder point)
Finds index of
SectionLineSegmentPointBuilder object in the list
License requirements: drafting ("DRAFTING") Created in NX10.0.0 |
void |
SectionLineSegmentPointListBuilder.insert(int insertBeforeIndex,
SectionLineSegmentPointBuilder point)
Inserts
SectionLineSegmentPointBuilder object in the list
before a given position
License requirements: drafting ("DRAFTING") Created in NX10.0.0 |
void |
SectionLineSegmentPointListBuilder.moveSegment(SectionLineSegmentPointBuilder point,
Point pointspecified)
Moves a given
SectionLineSegmentPointBuilder object from the list
License requirements: drafting ("DRAFTING") Created in NX10.0.0 |
void |
SectionLineSegmentPointListBuilder.setContents(SectionLineSegmentPointBuilder[] points)
Sets array of
SectionLineSegmentPointBuilder objects in the list. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.