Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static HingeLineBuilder.Hingeline |
HingeLineBuilder.Hingeline.DEFINED
The option for selecting hinge line using vector construction tools
|
static HingeLineBuilder.Hingeline |
HingeLineBuilder.Hingeline.INFERRED
The option to infer a hinge line based on parent, child view position
|
Modifier and Type | Method and Description |
---|---|
static HingeLineBuilder.Hingeline |
HingeLineBuilder.Hingeline.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HingeLineBuilder.Hingeline |
HingeLineBuilder.Hingeline.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HingeLineBuilder.Hingeline[] |
HingeLineBuilder.Hingeline.values()
Returns an array that contains the values for this enum.
|
HingeLineBuilder.Hingeline |
HingeLineBuilder.vectorOption()
Returns the vector option: Inferred or Defined
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
HingeLineBuilder.setVectorOption(HingeLineBuilder.Hingeline vectorOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.