Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static GeneralWorkFlowBuilder.GridSettingsType |
GeneralWorkFlowBuilder.GridSettingsType.DRAFTING |
static GeneralWorkFlowBuilder.GridSettingsType |
GeneralWorkFlowBuilder.GridSettingsType.SHEET_ZONE |
static GeneralWorkFlowBuilder.GridSettingsType |
GeneralWorkFlowBuilder.GridSettingsType.SKETCH |
Modifier and Type | Method and Description |
---|---|
GeneralWorkFlowBuilder.GridSettingsType |
GeneralWorkFlowBuilder.gridSettings()
Returns the option that indicates the grid settings
License requirements: None. |
static GeneralWorkFlowBuilder.GridSettingsType |
GeneralWorkFlowBuilder.GridSettingsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeneralWorkFlowBuilder.GridSettingsType |
GeneralWorkFlowBuilder.GridSettingsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeneralWorkFlowBuilder.GridSettingsType[] |
GeneralWorkFlowBuilder.GridSettingsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeneralWorkFlowBuilder.setGridSettings(GeneralWorkFlowBuilder.GridSettingsType gridSettings)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.