Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static DrawingSheetBuilder.SheetOption |
DrawingSheetBuilder.SheetOption.CUSTOM_SIZE
a custom size drawing sheet
|
static DrawingSheetBuilder.SheetOption |
DrawingSheetBuilder.SheetOption.STANDARD_SIZE
a standard size drawing sheet
|
static DrawingSheetBuilder.SheetOption |
DrawingSheetBuilder.SheetOption.USE_TEMPLATE
a drawing sheet template
|
Modifier and Type | Method and Description |
---|---|
DrawingSheetBuilder.SheetOption |
DrawingSheetBuilder.option()
Returns the option to be used to create the drawing sheet
License requirements: None. |
static DrawingSheetBuilder.SheetOption |
DrawingSheetBuilder.SheetOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawingSheetBuilder.SheetOption |
DrawingSheetBuilder.SheetOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawingSheetBuilder.SheetOption[] |
DrawingSheetBuilder.SheetOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawingSheetBuilder.setOption(DrawingSheetBuilder.SheetOption option)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.