Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static DrawingSheetBuilder.SheetBaseordrawingView |
DrawingSheetBuilder.SheetBaseordrawingView.BASE
auto start base view
|
static DrawingSheetBuilder.SheetBaseordrawingView |
DrawingSheetBuilder.SheetBaseordrawingView.DRAWING
auto start drawing view
|
Modifier and Type | Method and Description |
---|---|
DrawingSheetBuilder.SheetBaseordrawingView |
DrawingSheetBuilder.baseordrawingView()
Returns the option of base view or drawing view
License requirements: None. |
static DrawingSheetBuilder.SheetBaseordrawingView |
DrawingSheetBuilder.SheetBaseordrawingView.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawingSheetBuilder.SheetBaseordrawingView |
DrawingSheetBuilder.SheetBaseordrawingView.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawingSheetBuilder.SheetBaseordrawingView[] |
DrawingSheetBuilder.SheetBaseordrawingView.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawingSheetBuilder.setBaseordrawingView(DrawingSheetBuilder.SheetBaseordrawingView option)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.