Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Interface and Description |
---|---|
interface |
HalfPictorialSectionLine
Half Pictorial Section Line is used to create a pictorial view with
half of the part sectioned and the other half un-sectioned.
|
interface |
HalfSectionLine
Half Section Line is used to create a view with half of the part
sectioned and the other half un-sectioned.
|
interface |
SketchedHalfSectionLine
Sketched Half Section Line is sketch based section line.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.