Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static AnnotationSettingsBuilder.UnitsEnum |
AnnotationSettingsBuilder.UnitsEnum.USE_DRAWING_UNITS |
static AnnotationSettingsBuilder.UnitsEnum |
AnnotationSettingsBuilder.UnitsEnum.USE_TARGET_PART_UNITS |
Modifier and Type | Method and Description |
---|---|
AnnotationSettingsBuilder.UnitsEnum |
AnnotationSettingsBuilder.units()
Returns the units
License requirements: None. |
static AnnotationSettingsBuilder.UnitsEnum |
AnnotationSettingsBuilder.UnitsEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AnnotationSettingsBuilder.UnitsEnum |
AnnotationSettingsBuilder.UnitsEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AnnotationSettingsBuilder.UnitsEnum[] |
AnnotationSettingsBuilder.UnitsEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AnnotationSettingsBuilder.setUnits(AnnotationSettingsBuilder.UnitsEnum units)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.