public static class ViewPlacementBuilder.Option extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MODEL_POINT
Align to the same point in the alignment view and the view being edited
|
static int |
_POINT_TO_POINT
Align a point in the alignment view to another point in the view being edited
|
static int |
_TO_VIEW
Align to the view centers
|
static ViewPlacementBuilder.Option |
MODEL_POINT
Align to the same point in the alignment view and the view being edited
|
static ViewPlacementBuilder.Option |
POINT_TO_POINT
Align a point in the alignment view to another point in the view being edited
|
static ViewPlacementBuilder.Option |
TO_VIEW
Align to the view centers
|
Modifier and Type | Method and Description |
---|---|
static ViewPlacementBuilder.Option |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewPlacementBuilder.Option |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewPlacementBuilder.Option[] |
values()
Returns an array that contains the values for this enum.
|
public static final ViewPlacementBuilder.Option TO_VIEW
public static final ViewPlacementBuilder.Option MODEL_POINT
public static final ViewPlacementBuilder.Option POINT_TO_POINT
public static final int _TO_VIEW
public static final int _MODEL_POINT
public static final int _POINT_TO_POINT
public static ViewPlacementBuilder.Option valueOf(int value)
public static ViewPlacementBuilder.Option valueOf(String name)
public static ViewPlacementBuilder.Option[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.