public static class AssociativeAngleBuilder.ObjectType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_OBJECT
indicates the selected type is an object
|
static int |
_VECTOR
indicates the selected type is a vector
|
static AssociativeAngleBuilder.ObjectType |
OBJECT
indicates the selected type is an object
|
static AssociativeAngleBuilder.ObjectType |
VECTOR
indicates the selected type is a vector
|
Modifier and Type | Method and Description |
---|---|
static AssociativeAngleBuilder.ObjectType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssociativeAngleBuilder.ObjectType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssociativeAngleBuilder.ObjectType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AssociativeAngleBuilder.ObjectType OBJECT
public static final AssociativeAngleBuilder.ObjectType VECTOR
public static final int _OBJECT
public static final int _VECTOR
public static AssociativeAngleBuilder.ObjectType valueOf(int value)
public static AssociativeAngleBuilder.ObjectType valueOf(String name)
public static AssociativeAngleBuilder.ObjectType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.