public interface PointChildBuilder extends FeatureBuilder
Modifier and Type | Method and Description |
---|---|
DieBuildStatusOption |
buildStatus()
Returns the build status of the point.
|
boolean |
designStatus()
Returns the design status of the point, if true the point will be built into the model, if false it will not.
|
boolean |
displayStatus()
Returns the display status of the point, if true input data to the point will be displayed,
if false the input data will not be displayed.
|
Point |
point()
Returns the location of the point.
|
void |
setDesignStatus(boolean designStatus)
Sets the design status of the point, if true the point will be built into the model, if false it will not.
|
void |
setDisplayStatus(boolean displayStatus)
Sets the display status of the point, if true input data to the point will be displayed,
if false the input data will not be displayed.
|
void |
setPoint(Point point)
Sets the location of the point.
|
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
void setPoint(Point point) throws NXException, RemoteException
point
- NXException
RemoteException
Point point() throws NXException, RemoteException
NXException
RemoteException
void setDesignStatus(boolean designStatus) throws NXException, RemoteException
designStatus
- NXException
RemoteException
boolean designStatus() throws NXException, RemoteException
NXException
RemoteException
DieBuildStatusOption buildStatus() throws NXException, RemoteException
NXException
RemoteException
void setDisplayStatus(boolean displayStatus) throws NXException, RemoteException
displayStatus
- NXException
RemoteException
boolean displayStatus() throws NXException, RemoteException
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.