Package | Description |
---|---|
nxopen.diagramminglibraryauthor |
Provides classes and interfaces for Diagramming Library Authoring.
|
nxopen.pid |
Provides classes and interfaces for PID.
|
Modifier and Type | Method and Description |
---|---|
LineTypeBuilder |
LineTypeBuilderList.findItem(int index)
Returns the object at the input index.
|
LineTypeBuilder[] |
LineTypeBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
LineTypeBuilderList.append(LineTypeBuilder object)
Appends an object to the list
License requirements: None. |
void |
LineTypeBuilderList.append(LineTypeBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
LineTypeBuilderList.erase(LineTypeBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
LineTypeBuilderList.erase(LineTypeBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
LineTypeBuilderList.findIndex(LineTypeBuilder obj)
Finds the index where the input object appears.
|
void |
LineTypeBuilderList.insert(int location,
LineTypeBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
LineTypeBuilderList.setContents(LineTypeBuilder[] objects)
Sets the contents of the entire list.
|
void |
LineTypeBuilderList.swap(LineTypeBuilder object1,
LineTypeBuilder object2)
Exchanges the position of two objects inside the list.
|
Modifier and Type | Method and Description |
---|---|
LineTypeBuilder |
LibraryAuthoringBuilder.createLineType()
Creates a new line type
License requirements: nx_pid_design_author ("NX P and ID Design Author") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.