Package | Description |
---|---|
nxopen.diagramming.tables |
Provides classes and interfaces for Diagramming Tables.
|
Modifier and Type | Field and Description |
---|---|
static HeaderOrientation |
HeaderOrientation.HORIZONTAL
Horizontal header orientation
|
static HeaderOrientation |
HeaderOrientation.VERTICAL
Vertical header orientation
|
Modifier and Type | Method and Description |
---|---|
HeaderOrientation |
TableSettingsBuilder.headerOrientation()
Returns the header orientation of the table settings.
|
static HeaderOrientation |
HeaderOrientation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HeaderOrientation |
HeaderOrientation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HeaderOrientation[] |
HeaderOrientation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TableSettingsBuilder.setHeaderOrientation(HeaderOrientation headerOrientation)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.