Package | Description |
---|---|
nxopen.diagramming |
Provides classes and interfaces relating to Diagramming.
|
Modifier and Type | Method and Description |
---|---|
PortBuilder |
PortCollection.createPortBuilder(Port port)
Creates a
PortBuilder . |
PortBuilder |
PortBuilderList.findItem(int index)
Returns the object at the input index.
|
PortBuilder[] |
PortBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PortBuilderList.append(PortBuilder object)
Appends an object to the list
License requirements: None. |
void |
PortBuilderList.append(PortBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PortBuilderList.erase(PortBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
PortBuilderList.erase(PortBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PortBuilderList.findIndex(PortBuilder obj)
Finds the index where the input object appears.
|
void |
PortBuilderList.insert(int location,
PortBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
PortBuilderList.setContents(PortBuilder[] objects)
Sets the contents of the entire list.
|
void |
PortBuilderList.swap(PortBuilder object1,
PortBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.