Package | Description |
---|---|
nxopen.diagramming |
Provides classes and interfaces relating to Diagramming.
|
Modifier and Type | Method and Description |
---|---|
LeaderLineBuilder |
CannedAnnotationBuilder.createLeaderLine()
Create a new
LeaderLineBuilder builder. |
LeaderLineBuilder |
LeaderLineCollection.createLeaderLineBuilder(LeaderLine leaderLine)
Creates a
LeaderLineBuilder . |
LeaderLineBuilder |
LeaderLineBuilderList.findItem(int index)
Returns the object at the input index.
|
LeaderLineBuilder[] |
LeaderLineBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
LeaderLineBuilderList.append(LeaderLineBuilder object)
Appends an object to the list
License requirements: None. |
void |
LeaderLineBuilderList.append(LeaderLineBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
LeaderLineBuilderList.erase(LeaderLineBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
LeaderLineBuilderList.erase(LeaderLineBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
LeaderLineBuilderList.findIndex(LeaderLineBuilder obj)
Finds the index where the input object appears.
|
void |
LeaderLineBuilderList.insert(int location,
LeaderLineBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
LeaderLineBuilderList.setContents(LeaderLineBuilder[] objects)
Sets the contents of the entire list.
|
void |
LeaderLineBuilderList.swap(LeaderLineBuilder object1,
LeaderLineBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.