Package | Description |
---|---|
nxopen.diagramming |
Provides classes and interfaces relating to Diagramming.
|
Modifier and Type | Field and Description |
---|---|
static LeaderLineBuilder.VerticalAlignmentOption |
LeaderLineBuilder.VerticalAlignmentOption.BOTTOM
Setting the vertical alignment bottom
|
static LeaderLineBuilder.VerticalAlignmentOption |
LeaderLineBuilder.VerticalAlignmentOption.MIDDLE
Setting the vertical alignment middle
|
static LeaderLineBuilder.VerticalAlignmentOption |
LeaderLineBuilder.VerticalAlignmentOption.TOP
Setting the vertical alignment top
|
Modifier and Type | Method and Description |
---|---|
static LeaderLineBuilder.VerticalAlignmentOption |
LeaderLineBuilder.VerticalAlignmentOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LeaderLineBuilder.VerticalAlignmentOption |
LeaderLineBuilder.VerticalAlignmentOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LeaderLineBuilder.VerticalAlignmentOption[] |
LeaderLineBuilder.VerticalAlignmentOption.values()
Returns an array that contains the values for this enum.
|
LeaderLineBuilder.VerticalAlignmentOption |
LeaderLineBuilder.verticalAlignment()
Returns the vertical alignment option.
|
Modifier and Type | Method and Description |
---|---|
void |
LeaderLineBuilder.setVerticalAlignment(LeaderLineBuilder.VerticalAlignmentOption alignmentOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.