Package | Description |
---|---|
nxopen.diagramming |
Provides classes and interfaces relating to Diagramming.
|
Modifier and Type | Field and Description |
---|---|
static DiagrammingArrowtype |
DiagrammingArrowtype.CLOSED_SOLID
Setting the arrow type closed solid arrow
|
static DiagrammingArrowtype |
DiagrammingArrowtype.FILLED
Setting the arrow type filled arrow
|
static DiagrammingArrowtype |
DiagrammingArrowtype.NONE
Setting the arrow type none arrow
|
static DiagrammingArrowtype |
DiagrammingArrowtype.OPEN
Setting the arrow type open arrow
|
Modifier and Type | Method and Description |
---|---|
DiagrammingArrowtype |
LeaderLineBuilder.arrowType()
Returns the arrow type of the end arrow
License requirements: None. |
static DiagrammingArrowtype |
DiagrammingArrowtype.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DiagrammingArrowtype |
DiagrammingArrowtype.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DiagrammingArrowtype[] |
DiagrammingArrowtype.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LeaderLineBuilder.setArrowType(DiagrammingArrowtype arrowTypeOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.