Package | Description |
---|---|
nxopen.diagramming |
Provides classes and interfaces relating to Diagramming.
|
Modifier and Type | Field and Description |
---|---|
static DiagrammingAnnotationboundarytype |
DiagrammingAnnotationboundarytype.CIRCLE
Circle Type
|
static DiagrammingAnnotationboundarytype |
DiagrammingAnnotationboundarytype.ELLIPSE
Ellipse Type
|
static DiagrammingAnnotationboundarytype |
DiagrammingAnnotationboundarytype.NONE
No Boundary Type
|
static DiagrammingAnnotationboundarytype |
DiagrammingAnnotationboundarytype.RECTANGLE
Rectangle Type
|
static DiagrammingAnnotationboundarytype |
DiagrammingAnnotationboundarytype.ROUNDED_RECTANGLE
Rounded Rectangle Type
|
Modifier and Type | Method and Description |
---|---|
DiagrammingAnnotationboundarytype |
AnnotationBuilder.boundaryType()
Returns the boundary type of the annotation
License requirements: None. |
static DiagrammingAnnotationboundarytype |
DiagrammingAnnotationboundarytype.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DiagrammingAnnotationboundarytype |
DiagrammingAnnotationboundarytype.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DiagrammingAnnotationboundarytype[] |
DiagrammingAnnotationboundarytype.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AnnotationBuilder.setBoundaryType(DiagrammingAnnotationboundarytype boundaryType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.