Package | Description |
---|---|
nxopen.diagramming |
Provides classes and interfaces relating to Diagramming.
|
Modifier and Type | Method and Description |
---|---|
ConnectionLocationBuilder |
ConnectionLocationBuilderList.findItem(int index)
Returns the object at the input index.
|
ConnectionLocationBuilder[] |
ConnectionLocationBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ConnectionLocationBuilderList.append(ConnectionLocationBuilder object)
Appends an object to the list
License requirements: None. |
void |
ConnectionLocationBuilderList.append(ConnectionLocationBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ConnectionLocationBuilderList.erase(ConnectionLocationBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ConnectionLocationBuilderList.erase(ConnectionLocationBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ConnectionLocationBuilderList.findIndex(ConnectionLocationBuilder obj)
Finds the index where the input object appears.
|
void |
ConnectionLocationBuilderList.insert(int location,
ConnectionLocationBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ConnectionLocationBuilderList.setContents(ConnectionLocationBuilder[] objects)
Sets the contents of the entire list.
|
void |
ConnectionLocationBuilderList.swap(ConnectionLocationBuilder object1,
ConnectionLocationBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.