Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Validation.UpdateTime |
Validation.UpdateTime.EVERY_CHANGE
Every update when the input was changed
|
static Validation.UpdateTime |
Validation.UpdateTime.SAVE
During save time
|
Modifier and Type | Method and Description |
---|---|
static Validation.UpdateTime |
Validation.UpdateTime.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Validation.UpdateTime |
Validation.UpdateTime.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Validation.UpdateTime[] |
Validation.UpdateTime.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Validation.setUpdateControl(Validation.UpdateTime updateTime)
Define the update behavior of the validation object
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.