Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Validation.InputType |
Validation.InputType.APPLICATION
Input rules are from validation applications
|
static Validation.InputType |
Validation.InputType.KF_CLASS
Input rules are in a KF class
|
static Validation.InputType |
Validation.InputType.NUM
Last item define the number of the input source, not used as a type.
|
static Validation.InputType |
Validation.InputType.SPREADSHEET
Input rules are from a spreadsheet
|
static Validation.InputType |
Validation.InputType.TCR
Input rules are from TcR
|
static Validation.InputType |
Validation.InputType.TEXT_FILE
Input rules are from a text file
|
static Validation.InputType |
Validation.InputType.XML
Input rules are from XML file
|
Modifier and Type | Method and Description |
---|---|
static Validation.InputType |
Validation.InputType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Validation.InputType |
Validation.InputType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Validation.InputType[] |
Validation.InputType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
Validation |
ValidationCollection.create(String source,
Validation.InputType type)
Create a new validation object
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.