Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static StepCreator.ExportAsOption |
StepCreator.ExportAsOption.AP203
export using AP203
|
static StepCreator.ExportAsOption |
StepCreator.ExportAsOption.AP214
export using AP214
|
static StepCreator.ExportAsOption |
StepCreator.ExportAsOption.AP242
export using AP242
|
Modifier and Type | Method and Description |
---|---|
StepCreator.ExportAsOption |
StepCreator.exportAs()
Returns the export as - this option will determine if data needs to be exported using AP203 or AP214 or AP242
License requirements: None. |
static StepCreator.ExportAsOption |
StepCreator.ExportAsOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepCreator.ExportAsOption |
StepCreator.ExportAsOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepCreator.ExportAsOption[] |
StepCreator.ExportAsOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StepCreator.setExportAs(StepCreator.ExportAsOption exportAs)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.