Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static SpreadsheetManager.LookupMode |
SpreadsheetManager.LookupMode.CLOSEST
Returns the closest cell
|
static SpreadsheetManager.LookupMode |
SpreadsheetManager.LookupMode.EXACT
Requires an exact match
|
static SpreadsheetManager.LookupMode |
SpreadsheetManager.LookupMode.HIGHER
Returns the higher cell
|
static SpreadsheetManager.LookupMode |
SpreadsheetManager.LookupMode.LOWER
Returns the lower cell
|
Modifier and Type | Method and Description |
---|---|
static SpreadsheetManager.LookupMode |
SpreadsheetManager.LookupMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpreadsheetManager.LookupMode |
SpreadsheetManager.LookupMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpreadsheetManager.LookupMode[] |
SpreadsheetManager.LookupMode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
SpreadsheetCellData |
SpreadsheetManager.horizontalLookup(String file,
String target,
String range,
int offset,
SpreadsheetManager.LookupMode mode)
Reads the value from a given spreadsheet using a horizontal table lookup.
|
SpreadsheetCellData |
SpreadsheetManager.verticalLookup(String file,
String target,
String range,
int offset,
SpreadsheetManager.LookupMode mode)
Reads the value from a given spreadsheet using a vertical table lookup.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.