Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static SketchProjectBuilder.OutputCurve |
SketchProjectBuilder.OutputCurve.ORIGINAL
original curve output
|
static SketchProjectBuilder.OutputCurve |
SketchProjectBuilder.OutputCurve.SINGLE_SPLINE
single spline output
|
static SketchProjectBuilder.OutputCurve |
SketchProjectBuilder.OutputCurve.SPLINE_SEGMENT
spline segment output
|
Modifier and Type | Method and Description |
---|---|
SketchProjectBuilder.OutputCurve |
SketchProjectBuilder.curveType()
Returns the output curve type generated by the projection.
|
static SketchProjectBuilder.OutputCurve |
SketchProjectBuilder.OutputCurve.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchProjectBuilder.OutputCurve |
SketchProjectBuilder.OutputCurve.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchProjectBuilder.OutputCurve[] |
SketchProjectBuilder.OutputCurve.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SketchProjectBuilder.setCurveType(SketchProjectBuilder.OutputCurve curveType)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.