Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static SketchPattern.InstanceControl |
SketchPattern.InstanceControl.FULL_CIRCLE
The pattern instance control type is Full Circle
|
static SketchPattern.InstanceControl |
SketchPattern.InstanceControl.NUMBER_OFFSET
The pattern instance control type is number + offset
|
Modifier and Type | Method and Description |
---|---|
static SketchPattern.InstanceControl |
SketchPattern.InstanceControl.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchPattern.InstanceControl |
SketchPattern.InstanceControl.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchPattern.InstanceControl[] |
SketchPattern.InstanceControl.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.