Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static SketchOffset.CapType |
SketchOffset.CapType.ARC
The cap type is arc cap
|
static SketchOffset.CapType |
SketchOffset.CapType.EXTENSION
The cap type is curve extension
|
Modifier and Type | Method and Description |
---|---|
SketchOffset.CapType |
SketchOffsetBuilder.capType()
Returns the type of the cap needed at the corners
License requirements: None. |
static SketchOffset.CapType |
SketchOffset.CapType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchOffset.CapType |
SketchOffset.CapType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchOffset.CapType[] |
SketchOffset.CapType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SketchOffsetBuilder.setCapType(SketchOffset.CapType capType)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.