Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static SketchAlignmentConstraint.Type |
SketchAlignmentConstraint.Type.HORIZONTAL
The two vertices are horizontally aligned
|
static SketchAlignmentConstraint.Type |
SketchAlignmentConstraint.Type.VERTICAL
The two vertices are vertically aligned
|
Modifier and Type | Method and Description |
---|---|
SketchAlignmentConstraint.Type |
SketchAlignmentConstraint.alignmentType()
Returns the alignment type of the constraint.
|
static SketchAlignmentConstraint.Type |
SketchAlignmentConstraint.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchAlignmentConstraint.Type |
SketchAlignmentConstraint.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchAlignmentConstraint.Type[] |
SketchAlignmentConstraint.Type.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.