Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Sketch.UpdateLevel |
Sketch.UpdateLevel.MODEL
Update the full model and the sketch
|
static Sketch.UpdateLevel |
Sketch.UpdateLevel.SKETCH_ONLY
Only update the sketch
|
Modifier and Type | Method and Description |
---|---|
Sketch.UpdateLevel |
Sketch.updateScope()
Returns the current update scope.
|
static Sketch.UpdateLevel |
Sketch.UpdateLevel.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.UpdateLevel |
Sketch.UpdateLevel.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.UpdateLevel[] |
Sketch.UpdateLevel.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Sketch.deactivate(Sketch.ViewReorient orientView,
Sketch.UpdateLevel updateLevel)
Deactivates the sketch
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
void |
Sketch.setUpdateScope(Sketch.UpdateLevel updateScope)
Sets the current update scope.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.