Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Sketch.Status |
Sketch.Status.INCONSISTENTLY_CONSTRAINED
The sketch has conflicting constraints
|
static Sketch.Status |
Sketch.Status.NOT_EVALUATED |
static Sketch.Status |
Sketch.Status.OVER_CONSTRAINED
The sketch has more constraints than is needed
|
Sketch.Status |
Sketch.StatusData.status
The sketch's status, which indicates how well constrained the sketch is
|
static Sketch.Status |
Sketch.Status.UNDER_CONSTRAINED
More constraints are needed to fully constrain the sketch
|
static Sketch.Status |
Sketch.Status.UNKNOWN |
static Sketch.Status |
Sketch.Status.WELL_CONSTRAINED
The sketch is fully constrained
|
Modifier and Type | Method and Description |
---|---|
static Sketch.Status |
Sketch.Status.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.Status |
Sketch.Status.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.Status[] |
Sketch.Status.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.