Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Sketch.InferConstraintsOption |
Sketch.InferConstraintsOption.INFER_COINCIDENT_CONSTRAINTS
Infer constraints
|
static Sketch.InferConstraintsOption |
Sketch.InferConstraintsOption.INFER_NO_CONSTRAINTS
Do not infer constraints
|
Modifier and Type | Method and Description |
---|---|
static Sketch.InferConstraintsOption |
Sketch.InferConstraintsOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.InferConstraintsOption |
Sketch.InferConstraintsOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.InferConstraintsOption[] |
Sketch.InferConstraintsOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Sketch.addGeometry(Curve crv,
Sketch.InferConstraintsOption inferCoincidentConstraints,
Sketch.AddEllipseOption ellipseOption)
Adds a curve or point to a sketch.
|
void |
Sketch.addGeometry(DisplayableObject crv,
Sketch.InferConstraintsOption inferCoincidentConstraints)
Adds a curve or point to the sketch
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
void |
Sketch.addGeometry(Sketch.InferConstraintsOption inferCoincidentConstraints,
Sketch.AddEllipseOption ellipseOption,
SmartObject[] curvesOrPoints)
Adds an array of curves or points to a sketch.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.