Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Sketch.AddEllipseOption |
Sketch.AddEllipseOption.TREAT_AS_CONIC |
static Sketch.AddEllipseOption |
Sketch.AddEllipseOption.TREAT_AS_ELLIPSE |
Modifier and Type | Method and Description |
---|---|
static Sketch.AddEllipseOption |
Sketch.AddEllipseOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.AddEllipseOption |
Sketch.AddEllipseOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.AddEllipseOption[] |
Sketch.AddEllipseOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Sketch.addGeometry(Curve crv,
Sketch.InferConstraintsOption inferCoincidentConstraints,
Sketch.AddEllipseOption ellipseOption)
Adds a curve or point to a sketch.
|
void |
Sketch.addGeometry(Sketch.InferConstraintsOption inferCoincidentConstraints,
Sketch.AddEllipseOption ellipseOption,
SmartObject[] curvesOrPoints)
Adds an array of curves or points to a sketch.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.