Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Selection.UistylerSelectionType |
Selection.UistylerSelectionType.INACTIVE_SELECTION
sets selection inactive until
this function is called again
|
static Selection.UistylerSelectionType |
Selection.UistylerSelectionType.RECTANGLE_POSITION
the position is returned if no object is selected with the
single select gesture
|
static Selection.UistylerSelectionType |
Selection.UistylerSelectionType.ROBUST_SELECTION
reselect last
|
static Selection.UistylerSelectionType |
Selection.UistylerSelectionType.SINGLE_DESELECTION
single deselect
|
static Selection.UistylerSelectionType |
Selection.UistylerSelectionType.SINGLE_POSITION
the position is returned if no object is selected with the
single select gesture
|
static Selection.UistylerSelectionType |
Selection.UistylerSelectionType.SINGLE_SELECTION
allows
single select
|
Modifier and Type | Method and Description |
---|---|
static Selection.UistylerSelectionType |
Selection.UistylerSelectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Selection.UistylerSelectionType |
Selection.UistylerSelectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Selection.UistylerSelectionType[] |
Selection.UistylerSelectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Selection.setSelectType(SelectionHandle select,
Selection.UistylerSelectionType type)
Sets the selection type.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.