Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static SectionCollection.LoopOption |
SectionCollection.LoopOption.SEPARATE
One section is created for each loop
|
static SectionCollection.LoopOption |
SectionCollection.LoopOption.SEPARATE_OUTER
One section per outer loop and enclosed inner loops
|
Modifier and Type | Method and Description |
---|---|
static SectionCollection.LoopOption |
SectionCollection.LoopOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionCollection.LoopOption |
SectionCollection.LoopOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionCollection.LoopOption[] |
SectionCollection.LoopOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
Section[] |
SectionCollection.createSectionsUsingCurves(NXObject[] curves,
SectionCollection.LoopOption loopOption,
double chainingTolerance,
double distanceTolerance,
double angleTolerance)
Creates sections using curves such that each section can be extruded to produce one body.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.