Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static PropertyContainer.ListMode |
PropertyContainer.ListMode.INDEXED
The properties are not named and
must be indexed through an integer index
|
static PropertyContainer.ListMode |
PropertyContainer.ListMode.NAMED
The properties are named
|
Modifier and Type | Method and Description |
---|---|
PropertyContainer.ListMode |
PropertyContainer.mode()
Returns the mode of the list
License requirements: None. |
static PropertyContainer.ListMode |
PropertyContainer.ListMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PropertyContainer.ListMode |
PropertyContainer.ListMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PropertyContainer.ListMode[] |
PropertyContainer.ListMode.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.