Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.BINORMAL
Binormal to path, = FRENET_BINORMAL
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.NORMAL
Normal to path, = FRENET_NORMAL
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.NORMAL_TO_VECTOR
Normal to a vector
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.NOT_SPECIFIED
Subtype is not specified
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.PARALLEL_TO_VECTOR
Parallel to a vector
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.PROJECT
Reference to an object, = FRENET_PROJECT
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.TANGENT
Tangent to path, = FRENET_TANGENT
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.THRU_AXIS
Thru axis type
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.THRU_POINT
Thru point type and normal to path
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.THRU_POINT_BINORMAL
Thru point and binormal to path
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.THRU_POINT_NORMAL
Thru point and tangent_to_path
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.THRU_POINT_NORMAL_TO_VECTOR
Thru point and normal to a vector
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.THRU_POINT_PARALLEL_TO_VECTOR
Thru point and parallel to a vector
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.THRU_POINT_PROJECT
Thru point and relative to object
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.THRU_POINT_THRU_AXIS
Thru point and thru axis type
|
Modifier and Type | Method and Description |
---|---|
PlaneTypes.FrenetSubtype |
IPlane.frenetSubtype()
Returns the subtype of on curve type of plane fron NX6 onwards.
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlaneTypes.FrenetSubtype |
PlaneTypes.FrenetSubtype.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlaneTypes.FrenetSubtype[] |
PlaneTypes.FrenetSubtype.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IPlane.setFrenetSubtype(PlaneTypes.FrenetSubtype subtype)
Sets subtype for a specific plane type where the alternate solution cannot handle.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.