Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static PartCollection.SdpsStatus |
PartCollection.SdpsStatus.DRAWING_DISPLAYED
A drawing is currently displayed
|
static PartCollection.SdpsStatus |
PartCollection.SdpsStatus.GDT
The Tolerancing module is active
|
static PartCollection.SdpsStatus |
PartCollection.SdpsStatus.IN_PARTS_LIST
The Part List module is active
|
static PartCollection.SdpsStatus |
PartCollection.SdpsStatus.OK
The work part was set successfully.
|
static PartCollection.SdpsStatus |
PartCollection.SdpsStatus.OUTSIDE_MODELLING
The modelling application is not active
|
PartCollection.SdpsStatus |
PartCollection.SetDisplayData.status
Returns OK if the work part could be set as requested, or a status code
indicating the reason why this was not possible.
|
static PartCollection.SdpsStatus |
PartCollection.SdpsStatus.UNITS_MISMATCH
The work part and displayed part have different units
|
Modifier and Type | Method and Description |
---|---|
static PartCollection.SdpsStatus |
PartCollection.SdpsStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartCollection.SdpsStatus |
PartCollection.SdpsStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartCollection.SdpsStatus[] |
PartCollection.SdpsStatus.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.