Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static OriginMethod |
OriginMethod.SPECIFY_POINT
Specify Point
|
static OriginMethod |
OriginMethod.WORK_PART_ORIGIN
Use Work Part Origin
|
Modifier and Type | Method and Description |
---|---|
OriginMethod |
SketchInPlaceBuilder.originOption()
Returns the origin method for sketch
License requirements: None. |
OriginMethod |
SketchInPlaceBuilder.originOptionInfer()
Returns the origin method for sketch
License requirements: None. |
static OriginMethod |
OriginMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OriginMethod |
OriginMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OriginMethod[] |
OriginMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SketchInPlaceBuilder.setOriginOption(OriginMethod method)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
void |
SketchInPlaceBuilder.setOriginOptionInfer(OriginMethod method)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.