Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.visualreporting |
Provides classes and interfaces for Visual Reporting.
|
Modifier and Type | Field and Description |
---|---|
NXObject.ComputationalTime |
NXObject.AttributeInformation.compTimeValue
Time/Date attribute value (the default value is returned when reading templates of non-set attributes).
|
Modifier and Type | Method and Description |
---|---|
NXObject.ComputationalTime |
NXObject.getComputationalTimeUserAttribute(String title,
int index)
Gets a time attribute by Title and array Index.
|
Modifier and Type | Method and Description |
---|---|
void |
NXObject.setTimeUserAttribute(String title,
int index,
NXObject.ComputationalTime value,
Update.Option option)
Creates or modifies a time attribute with the option to update or not.
|
Constructor and Description |
---|
AttributeInformation(NXObject.AttributeType typeInitial,
String categoryInitial,
String titleInitial,
String titleAliasInitial,
boolean booleanValueInitial,
int integerValueInitial,
double realValueInitial,
String stringValueInitial,
String timeValueInitial,
NXObject.ComputationalTime compTimeValueInitial,
String referenceValueInitial,
boolean inheritedInitial,
boolean isOverrideInitial,
boolean lockedInitial,
boolean ownedBySystemInitial,
boolean requiredInitial,
boolean unsetInitial,
boolean arrayInitial,
boolean pdmBasedInitial,
boolean notSavedInitial,
int arrayElementIndexInitial,
Unit unitInitial,
Expression expressionInitial)
Constructor for the AttributeInformation object.
|
Modifier and Type | Method and Description |
---|---|
NXObject.ComputationalTime |
VisualReportManager.GetDateTypePropertyValue.getDateTypePropertyValue(NXObject nxObject)
User defined method that is called when ask an date property value.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.